PositioningTaskBuilder Class¶
-
class
NXOpen.Assemblies.
PositioningTaskBuilder
¶ Bases:
NXOpen.Builder
Represents the class for positioning task builder
To create a new instance of this class, use
NXOpen.Assemblies.SubsetCollection.CreatePositioningTaskBuilder
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
ContextCollection | Returns the context collection |
OwningSubset | Returns or sets the owning subset. |
Tag | Returns the Tag for this object. |
WorkCollection | Returns the work collection |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ContextCollection¶
-
PositioningTaskBuilder.
ContextCollection
¶ Returns the context collection
-------------------------------------
Getter Method
Signature
ContextCollection()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX10.0.0.
License requirements: None.
OwningSubset¶
-
PositioningTaskBuilder.
OwningSubset
¶ Returns or sets the owning subset.
During creation set method should be called with the subset instance in which new
NXOpen.Assemblies.PositioningTask
has to be created. During edit operation set method should not be called. An error would be raised if during edit operation set method is called with a subset instance which is different from the owning subset instance ofNXOpen.Assemblies.PositioningTask
.-------------------------------------
Getter Method
Signature
OwningSubset()
Returns: Return type: NXOpen.Assemblies.Subset
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OwningSubset(subsetInstance)
Parameters: subsetInstance ( NXOpen.Assemblies.Subset
) – This parameter may not be None.New in version NX10.0.0.
License requirements: nx_4gd_integration (“4th Generation Design”)
WorkCollection¶
-
PositioningTaskBuilder.
WorkCollection
¶ Returns the work collection
-------------------------------------
Getter Method
Signature
WorkCollection()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
PositioningTaskBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.