PmiManager Class¶
-
class
NXOpen.Annotations.
PmiManager
¶ Bases:
object
Represents an object that manages PMI objects.
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
ApplyModelViewOrder | Applies a saved explicit order |
CopyDisplayInstanceObjects | Creates copies of input PMI Display Instance objects in the part. |
CopyObjects | Creates copies of input PMI objects in the part. |
CreateArbitraryAreaSeedBuilder | Creates a NXOpen.Annotations.ArbitraryAreaSeedBuilder @return |
CreateExplicitOrderBuilder | Creates a NXOpen.Annotations.PMIExplicitOrderBuilder @return |
CutDisplayInstanceObjects | Cuts the input PMI Display Instance objects in the part. |
DeleteReplaceAnnotation | Deletes or replaces one annotation with another. |
GetDisplayInstanceParent | Returns the PMI Display Instance parent. |
GetInheritParent | Returns the inherited PMI parent. |
IsEffectivityFiltered | The flag indicates whether the PMI is an effectivity filtered PMI because of assembly component configuration from managed environment @return |
IsInheritedPmi | The flag indicating whether the annotation is an inherited PMI on the drawing sheet/view. |
Resize | Resizes all PMI symbols displayed in the active view |
RestoreUnpastedObjects | Restores the unpasted PMI objects in the part. |
SaveModelViewOrder | Saves an explicit order defined by the user |
Method Detail¶
ApplyModelViewOrder¶
-
PmiManager.
ApplyModelViewOrder
¶ Applies a saved explicit order
Signature
ApplyModelViewOrder(savedOrderName)
Parameters: savedOrderName (str) – New in version NX9.0.0.
License requirements: geometric_tol (“GDT”)
CopyDisplayInstanceObjects¶
-
PmiManager.
CopyDisplayInstanceObjects
¶ Creates copies of input PMI Display Instance objects in the part.
Only PMI Display Instance objects which can be copied in the NX user interface will be copied.
Client must perform update :py:meth:`NXOpen.Update.DoUpdate`() after calling this method.
Signature
CopyDisplayInstanceObjects(inputObjects, view)
Parameters: - inputObjects (list of
NXOpen.Annotations.Annotation
) – PMI Display Instance objects to be copied - view (
NXOpen.View
) – View in which PMI Display Instance are copied.
Returns: Copies of PMI Display Instance objects
Return type: list of
NXOpen.Annotations.Annotation
New in version NX5.0.0.
License requirements: geometric_tol (“GDT”)
- inputObjects (list of
CopyObjects¶
-
PmiManager.
CopyObjects
¶ Creates copies of input PMI objects in the part.
Only PMI objects which can be copied in the NX user interface will be copied.
Client must perform update
NXOpen.Update.DoUpdate
after calling this method.Signature
CopyObjects(inputObjects)
Parameters: inputObjects (list of NXOpen.Annotations.Pmi
) – PMI objects to be copiedReturns: Copies of PMI objects Return type: list of NXOpen.Annotations.Pmi
New in version NX5.0.0.
License requirements: geometric_tol (“GDT”)
CreateArbitraryAreaSeedBuilder¶
-
PmiManager.
CreateArbitraryAreaSeedBuilder
¶ Creates a
NXOpen.Annotations.ArbitraryAreaSeedBuilder
Signature
CreateArbitraryAreaSeedBuilder()
Returns: Return type: NXOpen.Annotations.ArbitraryAreaSeedBuilder
New in version NX6.0.0.
License requirements: None.
CreateExplicitOrderBuilder¶
-
PmiManager.
CreateExplicitOrderBuilder
¶ Creates a
NXOpen.Annotations.PMIExplicitOrderBuilder
Signature
CreateExplicitOrderBuilder()
Returns: Return type: NXOpen.Annotations.PMIExplicitOrderBuilder
New in version NX9.0.0.
License requirements: None.
CutDisplayInstanceObjects¶
-
PmiManager.
CutDisplayInstanceObjects
¶ Cuts the input PMI Display Instance objects in the part.
Cut operation makes the PMI Display Instance object invisible in the view of cut and makes it visible in the view of paste. Only PMI Display Instance objects which can be cut in the NX user interface will be copied.
Client must perform update :py:meth:`NXOpen.Update.DoUpdate`() after calling this method.
Signature
CutDisplayInstanceObjects(inputObjects, cutViews, viewOfPaste)
Parameters: - inputObjects (list of
NXOpen.Annotations.Annotation
) – PMI Display Instance objects to be cut - cutViews (list of
NXOpen.View
) – List of cut views. Each PMI Display Instance object is cut from the corresponding view in the list. - viewOfPaste (
NXOpen.View
) – View in which PMI Display Instances are pasted.
New in version NX5.0.0.
License requirements: geometric_tol (“GDT”)
- inputObjects (list of
DeleteReplaceAnnotation¶
-
PmiManager.
DeleteReplaceAnnotation
¶ Deletes or replaces one annotation with another.
This will adjust the requirements ID of the annotation if one annotation replaces another. This method may be used in NX generated automation programs but it is not intended to be used in a customer written automation program.
Signature
DeleteReplaceAnnotation(oldAnnotation, newAnnotation)
Parameters: - oldAnnotation (
NXOpen.Annotations.Annotation
) –NXOpen.Annotations.Annotation
Annotation or Dimension Set to be deleted - newAnnotation (
NXOpen.Annotations.Annotation
) –NXOpen.Annotations.Annotation
to replace the deleted annootation, can be NULL
New in version NX6.0.0.
License requirements: None.
- oldAnnotation (
GetDisplayInstanceParent¶
-
PmiManager.
GetDisplayInstanceParent
¶ Returns the PMI Display Instance parent.
The parent is the PMI Object.
Signature
GetDisplayInstanceParent(displayInstance)
Parameters: displayInstance ( NXOpen.Annotations.Annotation
) – PMI Display InstanceReturns: Parent PMI object Return type: NXOpen.Annotations.Pmi
New in version NX5.0.0.
License requirements: None.
GetInheritParent¶
-
PmiManager.
GetInheritParent
¶ Returns the inherited PMI parent.
The parent is the PMI Display Instance in modeling.
Signature
GetInheritParent(inheritedPmi)
Parameters: inheritedPmi ( NXOpen.Annotations.Annotation
) – Inherited PMIReturns: Parent PMI Display Instance Return type: NXOpen.Annotations.Annotation
New in version NX5.0.0.
License requirements: None.
IsEffectivityFiltered¶
-
PmiManager.
IsEffectivityFiltered
¶ The flag indicates whether the PMI is an effectivity filtered PMI because of assembly component configuration from managed environment
Signature
IsEffectivityFiltered(object)
Parameters: object ( NXOpen.Annotations.Pmi
) – PMI object to examineReturns: Return type: bool New in version NX8.5.1.
License requirements: None.
IsInheritedPmi¶
-
PmiManager.
IsInheritedPmi
¶ The flag indicating whether the annotation is an inherited PMI on the drawing sheet/view.
Inherited PMI is the associative copy of the PMI display instance in modeling.
Signature
IsInheritedPmi(object)
Parameters: object ( NXOpen.Annotations.Annotation
) – Annotation to examineReturns: Return type: bool New in version NX5.0.0.
License requirements: None.
Resize¶
-
PmiManager.
Resize
¶ Resizes all PMI symbols displayed in the active view
Signature
Resize()
New in version NX8.0.0.
License requirements: geometric_tol (“GDT”)
RestoreUnpastedObjects¶
-
PmiManager.
RestoreUnpastedObjects
¶ Restores the unpasted PMI objects in the part.
This method is used by NX user interface to restore PMI objects that were cut but not pasted. If called by an automation program, this method can cause unexpected results.
Signature
RestoreUnpastedObjects()
New in version NX5.0.0.
License requirements: geometric_tol (“GDT”)