PmiFilter Class¶
-
class
NXOpen.Annotations.
PmiFilter
¶ Bases:
NXOpen.NXObject
Represents a base class for a PMI filter.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ApplyToView | Applies the PMI filter to a view. |
Copy | Creates a copy of the PMI filter @return |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes encountered with the given Type with option to update or not. |
EnableInView | Enables or disables the PMI filter in a given view |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAppliedViews | Gets the views where the PMI filter is applied @return |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComponentMethod | Gets the component method of the PMI filter. |
GetComponents | Gets the components associated with the PMI filter. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetFilterType | Gets the type of PMI filter. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, of the given type. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute with the given Title, Type and array Index is present on the object Unset attributes will not be detected by this function, as its purpose is to test for the actual presence of the attribute on the object. |
IsEnabled | Determines if the PMI filter is enabled in the view @return |
Prints a representation of this object to the system log file. | |
RemoveFromView | Removes a PMI filter from a view. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetComponentMethod | Sets the component method of the PMI filter. |
SetComponents | Sets the components associated with the PMI filter. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
UpdatePmiDisplay | Updates the PMI display in the associated views of the filter |
Enumerations¶
PmiFilterComponentMethod Enumeration | Specifies the type of component method used on the associated components for display. |
PmiFilterFilterType Enumeration | Represents a type of PMI filter that can be created using the Part Navigator. |
Property Detail¶
IsOccurrence¶
-
PmiFilter.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
PmiFilter.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
PmiFilter.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
PmiFilter.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
PmiFilter.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
PmiFilter.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
ApplyToView¶
-
PmiFilter.
ApplyToView
¶ Applies the PMI filter to a view.
Signature
ApplyToView(view)
Parameters: view ( NXOpen.View
) – Specifies the model view in which the filter is to be appliedNew in version NX4.0.0.
License requirements: geometric_tol (“GDT”)
Copy¶
-
PmiFilter.
Copy
¶ Creates a copy of the PMI filter
Signature
Copy()
Returns: Return type: NXOpen.Annotations.PmiFilter
New in version NX4.0.0.
License requirements: geometric_tol (“GDT”)
EnableInView¶
-
PmiFilter.
EnableInView
¶ Enables or disables the PMI filter in a given view
Signature
EnableInView(view, enabled)
Parameters: - view (
NXOpen.View
) – Specifies the model view in which the filter should be enabled or disabled - enabled (bool) – Specifies the flag indicating that the filter should be enabled
New in version NX4.0.0.
License requirements: geometric_tol (“GDT”)
- view (
FindObject¶
-
PmiFilter.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetAppliedViews¶
-
PmiFilter.
GetAppliedViews
¶ Gets the views where the PMI filter is applied
Signature
GetAppliedViews()
Returns: Return type: list of NXOpen.View
New in version NX4.0.0.
License requirements: None.
GetComponentMethod¶
-
PmiFilter.
GetComponentMethod
¶ Gets the component method of the PMI filter.
Signature
GetComponentMethod()
Returns: Return type: NXOpen.Annotations.PmiFilterComponentMethod
New in version NX4.0.0.
License requirements: None.
GetComponents¶
-
PmiFilter.
GetComponents
¶ Gets the components associated with the PMI filter.
Signature
GetComponents()
Returns: Return type: list of NXOpen.Assemblies.Component
New in version NX4.0.0.
License requirements: None.
GetFilterType¶
-
PmiFilter.
GetFilterType
¶ Gets the type of PMI filter.
Signature
GetFilterType()
Returns: Return type: NXOpen.Annotations.PmiFilterFilterType
New in version NX4.0.0.
License requirements: None.
IsEnabled¶
-
PmiFilter.
IsEnabled
¶ Determines if the PMI filter is enabled in the view
Signature
IsEnabled(view)
Parameters: view ( NXOpen.View
) – Specifies the model view to queryReturns: Return type: bool New in version NX4.0.0.
License requirements: None.
Print¶
-
PmiFilter.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
RemoveFromView¶
-
PmiFilter.
RemoveFromView
¶ Removes a PMI filter from a view.
Signature
RemoveFromView(view)
Parameters: view ( NXOpen.View
) – Specifies the model view in which the filter should be removedNew in version NX4.0.0.
License requirements: geometric_tol (“GDT”)
SetComponentMethod¶
-
PmiFilter.
SetComponentMethod
¶ Sets the component method of the PMI filter.
Signature
SetComponentMethod(componentMethod)
Parameters: componentMethod ( NXOpen.Annotations.PmiFilterComponentMethod
) –New in version NX4.0.0.
License requirements: geometric_tol (“GDT”)
SetComponents¶
-
PmiFilter.
SetComponents
¶ Sets the components associated with the PMI filter.
Signature
SetComponents(components)
Parameters: components (list of NXOpen.Assemblies.Component
) –New in version NX4.0.0.
License requirements: geometric_tol (“GDT”)
SetName¶
-
PmiFilter.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.