PmiFilterFilterType Enumeration¶
NXOpen.Annotations.PmiFilter.FilterType is an alias for NXOpen.Annotations.PmiFilterFilterType
-
class
NXOpen.Annotations.
PmiFilterFilterType
¶ Bases:
object
Represents a type of PMI filter that can be created using the Part Navigator.
Enum Members
Enum Member Enum Member Description ByType Specifies a PMI filter defined by a set of PMI typesByView Specifies a PMI filter defined by a set of component model viewsByComponent Specifies a PMI filter defined by a set of components-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-