LineWeldBuilder Class¶
-
class
NXOpen.Annotations.
LineWeldBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Annotations.LineWeldBuilder
To create a new instance of this class, use
NXOpen.Annotations.WeldCollection.CreateLineWeldBuilder
Default values.
Property Value ArrowSideWeldData.ContourSymbol None ArrowSideWeldData.FinishSymbol None ArrowSideWeldData.WeldSizeCode None ArrowSideWeldData.WeldSymbol None FieldWeld Plain FlipDirection False FlipHorizontal False FlipVertical False IdLine Plain Scale 1 StaggeredWeld NoStaggeredSymbol Tail NoTail WeldAlongContour None New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ArrowSideWeldData | Returns the NXOpen.Annotations.LineWeldDataBuilder for the arrow side of the weld symbol |
FieldWeld | Returns or sets the field indicating the weld is done at the field site |
FlipDirection | Returns or sets the flip direction for top seam |
FlipHorizontal | Returns or sets the flip horizontal direction for side seam |
FlipVertical | Returns or sets the flip vertical direction for side seam |
ForeshorteningSymbol | Returns the foreshortening symbol builder |
IdLine | Returns or sets the identification or reference line |
Inherit | Returns the weld symbol from which the style properties are inherited |
Leader | Returns the NXOpen.Annotations.LeaderBuilder for weld symbol |
Origin | Returns the NXOpen.Annotations.OriginBuilder for the weld symbol |
OtherSideWeldData | Returns the NXOpen.Annotations.LineWeldDataBuilder for the other side of the weld symbol |
Scale | Returns or sets the scaling factor for the welding symbol |
SideSeamObjects | Returns the side seam object |
SpaceFactor | Returns or sets the space factor for the welding symbol |
StaggeredWeld | Returns or sets the staggered weld |
Style | Returns the NXOpen.Annotations.StyleBuilder for the weld symbol |
Tag | Returns the Tag for this object. |
Tail | Returns or sets the weld tail |
TopSeamObject | Returns the top seam object |
WeldAlongContour | Returns or sets the weld along contour option |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetReference | Returns the reference or specification text @return |
InheritProperties | This inherits the properties from the existing weld symbol |
InheritPropertiesFromWeldFeature | This inherits the properties from the existing weld feature |
SetReference | Sets the reference or specification text |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LineWeldBuilderFieldWeldType Enumeration | Represents the field weld type |
LineWeldBuilderIdLineType Enumeration | Represents the id line type |
LineWeldBuilderStaggeredWeldType Enumeration | Represents the staggered weld type |
LineWeldBuilderTailType Enumeration | represents the tail type |
LineWeldBuilderWeldSymbolWeldAlongContourType Enumeration | Represents the weld along contour option |
Property Detail¶
ArrowSideWeldData¶
-
LineWeldBuilder.
ArrowSideWeldData
¶ Returns the
NXOpen.Annotations.LineWeldDataBuilder
for the arrow side of the weld symbol-------------------------------------
Getter Method
Signature
ArrowSideWeldData()
Returns: Return type: NXOpen.Annotations.LineWeldDataBuilder
New in version NX6.0.0.
License requirements: None.
FieldWeld¶
-
LineWeldBuilder.
FieldWeld
¶ Returns or sets the field indicating the weld is done at the field site
-------------------------------------
Getter Method
Signature
FieldWeld()
Returns: Return type: NXOpen.Annotations.LineWeldBuilderFieldWeldType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FieldWeld(fieldWeld)
Parameters: fieldWeld ( NXOpen.Annotations.LineWeldBuilderFieldWeldType
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
FlipDirection¶
-
LineWeldBuilder.
FlipDirection
¶ Returns or sets the flip direction for top seam
-------------------------------------
Getter Method
Signature
FlipDirection()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FlipDirection(flipDirection)
Parameters: flipDirection (bool) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
FlipHorizontal¶
-
LineWeldBuilder.
FlipHorizontal
¶ Returns or sets the flip horizontal direction for side seam
-------------------------------------
Getter Method
Signature
FlipHorizontal()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FlipHorizontal(flipHorizontal)
Parameters: flipHorizontal (bool) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
FlipVertical¶
-
LineWeldBuilder.
FlipVertical
¶ Returns or sets the flip vertical direction for side seam
-------------------------------------
Getter Method
Signature
FlipVertical()
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FlipVertical(flipVertical)
Parameters: flipVertical (bool) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
ForeshorteningSymbol¶
-
LineWeldBuilder.
ForeshorteningSymbol
¶ Returns the foreshortening symbol builder
-------------------------------------
Getter Method
Signature
ForeshorteningSymbol()
Returns: Return type: NXOpen.Annotations.ForeshorteningSymbolBuilder
New in version NX10.0.0.
License requirements: None.
IdLine¶
-
LineWeldBuilder.
IdLine
¶ Returns or sets the identification or reference line
-------------------------------------
Getter Method
Signature
IdLine()
Returns: Return type: NXOpen.Annotations.LineWeldBuilderIdLineType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IdLine(idLine)
Parameters: idLine ( NXOpen.Annotations.LineWeldBuilderIdLineType
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
Inherit¶
-
LineWeldBuilder.
Inherit
¶ Returns the weld symbol from which the style properties are inherited
-------------------------------------
Getter Method
Signature
Inherit()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX6.0.0.
License requirements: None.
Leader¶
-
LineWeldBuilder.
Leader
¶ Returns the
NXOpen.Annotations.LeaderBuilder
for weld symbol-------------------------------------
Getter Method
Signature
Leader()
Returns: Return type: NXOpen.Annotations.LeaderBuilder
New in version NX6.0.0.
License requirements: None.
Origin¶
-
LineWeldBuilder.
Origin
¶ Returns the
NXOpen.Annotations.OriginBuilder
for the weld symbol-------------------------------------
Getter Method
Signature
Origin()
Returns: Return type: NXOpen.Annotations.OriginBuilder
New in version NX6.0.0.
License requirements: None.
OtherSideWeldData¶
-
LineWeldBuilder.
OtherSideWeldData
¶ Returns the
NXOpen.Annotations.LineWeldDataBuilder
for the other side of the weld symbol-------------------------------------
Getter Method
Signature
OtherSideWeldData()
Returns: Return type: NXOpen.Annotations.LineWeldDataBuilder
New in version NX6.0.0.
License requirements: None.
Scale¶
-
LineWeldBuilder.
Scale
¶ Returns or sets the scaling factor for the welding symbol
-------------------------------------
Getter Method
Signature
Scale()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Scale(scale)
Parameters: scale (float) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
SideSeamObjects¶
-
LineWeldBuilder.
SideSeamObjects
¶ Returns the side seam object
-------------------------------------
Getter Method
Signature
SideSeamObjects()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX6.0.0.
License requirements: None.
SpaceFactor¶
-
LineWeldBuilder.
SpaceFactor
¶ Returns or sets the space factor for the welding symbol
-------------------------------------
Getter Method
Signature
SpaceFactor()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpaceFactor(spaceFactor)
Parameters: spaceFactor (float) – New in version NX7.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
StaggeredWeld¶
-
LineWeldBuilder.
StaggeredWeld
¶ Returns or sets the staggered weld
-------------------------------------
Getter Method
Signature
StaggeredWeld()
Returns: Return type: NXOpen.Annotations.LineWeldBuilderStaggeredWeldType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StaggeredWeld(staggeredWeld)
Parameters: staggeredWeld ( NXOpen.Annotations.LineWeldBuilderStaggeredWeldType
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
Style¶
-
LineWeldBuilder.
Style
¶ Returns the
NXOpen.Annotations.StyleBuilder
for the weld symbol-------------------------------------
Getter Method
Signature
Style()
Returns: Return type: NXOpen.Annotations.StyleBuilder
New in version NX6.0.0.
License requirements: None.
Tail¶
-
LineWeldBuilder.
Tail
¶ Returns or sets the weld tail
-------------------------------------
Getter Method
Signature
Tail()
Returns: Return type: NXOpen.Annotations.LineWeldBuilderTailType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tail(tail)
Parameters: tail ( NXOpen.Annotations.LineWeldBuilderTailType
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
TopSeamObject¶
-
LineWeldBuilder.
TopSeamObject
¶ Returns the top seam object
-------------------------------------
Getter Method
Signature
TopSeamObject()
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX6.0.0.
License requirements: None.
WeldAlongContour¶
-
LineWeldBuilder.
WeldAlongContour
¶ Returns or sets the weld along contour option
-------------------------------------
Getter Method
Signature
WeldAlongContour()
Returns: Return type: NXOpen.Annotations.LineWeldBuilderWeldSymbolWeldAlongContourType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WeldAlongContour(alongContour)
Parameters: alongContour ( NXOpen.Annotations.LineWeldBuilderWeldSymbolWeldAlongContourType
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
Method Detail¶
GetReference¶
-
LineWeldBuilder.
GetReference
¶ Returns the reference or specification text
Signature
GetReference()
Returns: Return type: list of str New in version NX6.0.0.
License requirements: None.
InheritProperties¶
-
LineWeldBuilder.
InheritProperties
¶ This inherits the properties from the existing weld symbol
Signature
InheritProperties(annotation)
Parameters: annotation ( NXOpen.Annotations.Weld
) –New in version NX8.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
InheritPropertiesFromWeldFeature¶
-
LineWeldBuilder.
InheritPropertiesFromWeldFeature
¶ This inherits the properties from the existing weld feature
Signature
InheritPropertiesFromWeldFeature(feature)
Parameters: feature ( NXOpen.Body
) –New in version NX8.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
SetReference¶
-
LineWeldBuilder.
SetReference
¶ Sets the reference or specification text
Signature
SetReference(reference)
Parameters: reference (list of str) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
Validate¶
-
LineWeldBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.