LeaderBuilder Class¶
-
class
NXOpen.Annotations.
LeaderBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.LeaderBuilder
.This class is used to construct a leader for an annotation object.
This is a sub-builder class and cannot be directly instantiated
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Leaders | Returns the leaders to attach to the annotation |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Leaders¶
-
LeaderBuilder.
Leaders
¶ Returns the leaders to attach to the annotation
-------------------------------------
Getter Method
Signature
Leaders()
Returns: Return type: NXOpen.Annotations.LeaderDataList
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
LeaderBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.