ComponentData Class¶
-
class
NXOpen.Annotations.
ComponentData
¶ Bases:
NXOpen.TransientObject
A ComponentData object can be used to query the components of an annotation.
These components include line components, arrow components, arc components, and text components. These components can then be queried for type specific information about the object. .. versionadded:: NX6.0.2
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetArcComponents | Queries the arc components, (NXOpen.Annotations.ArcComponent ), in an annotation. |
GetArrowComponents | Queries the arrow components, (NXOpen.Annotations.ArrowComponent ), in an annotation. |
GetEntities | Returns the entities that display the annotation. |
GetLineComponents | Queries the line components, (NXOpen.Annotations.LineComponent ), in an annotation. |
GetTextComponents | Queries the text components, (NXOpen.Annotations.ArcComponent ), in an annotation. |
Method Detail¶
Dispose¶
-
ComponentData.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX6.0.2.
License requirements: None.
GetArcComponents¶
-
ComponentData.
GetArcComponents
¶ Queries the arc components, (
NXOpen.Annotations.ArcComponent
), in an annotation.Each arc component can be queried for arc specific information.
Signature
GetArcComponents()
Returns: All of the arc components that exist in the annotation Return type: list of NXOpen.Annotations.ArcComponent
New in version NX6.0.2.
License requirements: None.
GetArrowComponents¶
-
ComponentData.
GetArrowComponents
¶ Queries the arrow components, (
NXOpen.Annotations.ArrowComponent
), in an annotation.Each arrow component can be queried for arrow specific information.
Signature
GetArrowComponents()
Returns: All of the arrow components that exist in the annotation Return type: list of NXOpen.Annotations.ArrowComponent
New in version NX6.0.2.
License requirements: None.
GetEntities¶
-
ComponentData.
GetEntities
¶ Returns the entities that display the annotation.
Each entity can be queried to get the line, arc and text information. Note that entities could be line, arc, spline and annotation objects.
Signature
GetEntities()
Returns: List of entities that display the annotation Return type: list of NXOpen.DisplayableObject
New in version NX6.0.2.
License requirements: None.
GetLineComponents¶
-
ComponentData.
GetLineComponents
¶ Queries the line components, (
NXOpen.Annotations.LineComponent
), in an annotation.Each line component can be queried for line specific information.
Signature
GetLineComponents()
Returns: All of the lines components that exist in the annotation Return type: list of NXOpen.Annotations.LineComponent
New in version NX6.0.2.
License requirements: None.
GetTextComponents¶
-
ComponentData.
GetTextComponents
¶ Queries the text components, (
NXOpen.Annotations.ArcComponent
), in an annotation.Each text component can be queried for text specific information.
Signature
GetTextComponents()
Returns: All of the text components that exist in the annotation Return type: list of NXOpen.Annotations.TextComponent
New in version NX6.0.2.
License requirements: None.