LineComponent Class¶
-
class
NXOpen.Annotations.
LineComponent
¶ Bases:
NXOpen.TransientObject
Represents a single line in an annotation and can be queried for information about that line.
This information includes the line type, the start point in absolute coordinates, and the end point in absolute coordinates. .. versionadded:: NX6.0.2
Properties¶
Property | Description |
---|---|
EndPoint | Returns the line end point in absolute coordinates. |
Index | Returns the line index. |
StartPoint | Returns the line start point in absolute coordinates. |
Type | Returns the line type. |
Enumerations¶
LineComponentLineType Enumeration | the line type |
Property Detail¶
EndPoint¶
-
LineComponent.
EndPoint
¶ Returns the line end point in absolute coordinates.
If the annotation is on a drawing, the end point is returned in drawing space. If the annotation is on the model, the end point is returned in model space.
-------------------------------------
Getter Method
Signature
EndPoint()
Returns: the line end point in absolute coordinates Return type: NXOpen.Point3d
New in version NX6.0.2.
License requirements: None.
Index¶
-
LineComponent.
Index
¶ Returns the line index.
-------------------------------------
Getter Method
Signature
Index()
Returns: the line index Return type: int New in version NX9.0.0.
License requirements: None.
StartPoint¶
-
LineComponent.
StartPoint
¶ Returns the line start point in absolute coordinates.
If the annotation is on a drawing, the start point is returned in drawing space. If the annotation is on the model, the start point is returned in model space.
-------------------------------------
Getter Method
Signature
StartPoint()
Returns: the line start point in absolute coordinates Return type: NXOpen.Point3d
New in version NX6.0.2.
License requirements: None.
Type¶
-
LineComponent.
Type
¶ Returns the line type.
-------------------------------------
Getter Method
Signature
Type()
Returns: the line type Return type: NXOpen.Annotations.LineComponentLineType
New in version NX6.0.2.
License requirements: None.
Method Detail¶
Dispose¶
-
LineComponent.
Dispose
¶ Free resources associated with the line component.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX6.0.2.
License requirements: None.