Business processes involving Teamcenter Manufacturing Access
Business process 1 – Process planning using Manufacturing Process Planner
When you prepare to do process planning using Manufacturing Process Planner, you need to use Teamcenter Manufacturing Access to create, search, and load studies.
Role
Task
Administrator
Administrators install and configure the environment and convert studies.
Process planner
Engineers in planning groups use the Teamcenter rich client to perform planning tasks. These tasks are performed in Teamcenter Manufacturing Process Planner. See the Manufacturing Process Planner documentation for details.
Business process 2 – Process plan validation using Process Simulate
When you prepare to do process validation using Process Simulate on Teamcenter, you need to use Teamcenter Manufacturing Access to create, search, and load studies. You also may need to insert additional resources or manufacturing features using Teamcenter Manufacturing Access.
Role
Task
Administrator
Administrators install and configure the environment and convert studies.
Simulation engineer
Engineers need to validate that the designed processes are doable. See the Process Simulate on Teamcenter documentation for details.
Business process 3 – Designing a fixture using NX Fixture Planner
When you prepare to do fixture planning using Manufacturing Process Planner, you need to use Teamcenter Manufacturing Access to create, search, and load studies.
Role
Task
Administrator
Administrators install and configure the environment and convert studies.
Fixture planner
Engineers need to use available information to design the fixtures used to manufacturer the product. See the NX Fixture Planner documentation for details.