Use Teamcenter Manufacturing Access while designing a fixture
When you perform fixture planning using NX, you need to create, search, and load studies.
Administrator
See the Teamcenter Manufacturing Access Deployment documentation.
Your administrator completes the following data setup steps:
Deploy your environment
Install and configure NX, Teamcenter, and Teamcenter Manufacturing Access.
Convert legacy studies
Convert studies created before using Teamcenter Manufacturing Access using a workflow.
Fixture planner
The fixture planner completes the following steps in NX:
Start NX in managed mode
See the NX documentation.
Search for a collaboration context using Study Manager, and review its studies.
Note:The Study Manager is available to NX Fixture Planner users with Teamcenter Manufacturing Access configured.
(Optional) Create a study
If after searching, you do not find a suitable study, create a study using the Study Manager.
Load a study using the Study Manager.
Use NX Fixture Planner to begin designing a fixture.
See the NX Fixture Planner documentation.