Solid Edge Part Type Library
put_CloseBoundaryOption Method
Description
Put close boundary option.
Syntax
Visual Basic
Public Sub put_CloseBoundaryOption( _
   ByVal CloseBoundaryOption As Long _
) 
Parameters
CloseBoundaryOption
Example
Private Sub CloseBoundaryOption_Click(sender As Object, e As EventArgs) Handles PuCloseBoundaryOption.Click
    Dim objApplication As SolidEdgeFramework.Application
    Dim objPartDoc As SolidEdgePart.PartDocument = Nothing
    Dim objConstructions As SolidEdgePart.Constructions = Nothing
    Dim objBdrySurfaces As SolidEdgePart.SurfaceByBoundaries = Nothing
    Dim objBdrySurface As SolidEdgePart.SurfaceByBoundary = Nothing
    Dim objProfileSet As SolidEdgePart.ProfileSet = Nothing
    Dim objProfile As SolidEdgePart.Profile = Nothing
    Dim sketch As SolidEdgePart.Sketch = Nothing
    Dim arrInEdges(0 To 3) As Object
    Dim arrGuideWire(0 To 1) As Object
    Dim arrInEdgesForTangentTypes(1) As Object
    Dim arrTangentTypes(3) As SolidEdgeConstants.SurfaceByBoundaryTangencyType
    Dim arrTangentFace(3) As Object
    Dim bCloseBounaryOption As Boolean
    Dim arrOutEdgesForTangentTypes(3) As Object
    Dim arrOutTangentTypes(3) As SolidEdgeConstants.SurfaceByBoundaryTangencyType

    Try
        ' Create/get the application with specific settings
        objApplication = Marshal.GetActiveObject("SolidEdge.Application")

        ' Get the document
        objPartDoc = objApplication.ActiveDocument

        ' get the constructions collection
        objConstructions = objPartDoc.Constructions
        objBdrySurfaces = objConstructions.SurfaceByBoundaries

        ' input edges
        sketch = objPartDoc.Sketches.Item(1)
        objProfile = sketch.Profile

        ' get input edges to create bounded surface
        arrInEdges(0) = objProfile.CurveBody.Curves.Item(1)
        arrInEdges(1) = objProfile.CurveBody.Curves.Item(2)
        arrInEdges(2) = objProfile.CurveBody.Curves.Item(3)
        arrInEdges(3) = objProfile.CurveBody.Curves.Item(4)

        'Create the SurfaceByBoundary using Add3()
        'All boundary edges with natural continuity therefore NumberOfEdgesForTangentTypes and NumberOfTangentFaces are passed as zero.

        arrGuideWire(0) = objPartDoc.Sketches.Item(2).Profile.CurveBody.Curves.Item(1)

        objBdrySurface = objBdrySurfaces.Add3(4, arrInEdges, 0, arrInEdgesForTangentTypes, arrTangentTypes, 0, arrTangentFace, 1, arrGuideWire, False, SolidEdgeConstants.SurfaceByBoundaryPatchTopology.igSurfaceByBoundaryMultiple)
        'Test get and set of close boundary option.
        objBdrySurface.get_CloseBoundaryOption(bCloseBounaryOption)
        'Set the option as false, so with only 3 open edges feature should fail.
        bCloseBounaryOption = False
        objBdrySurface.put_CloseBoundaryOption(bCloseBounaryOption)



    Catch ex As Exception
        MsgBox(ex.ToString)
    End Try
End Sub
See Also

SurfaceByBoundary Object  | SurfaceByBoundary Members