Solid Edge Part Type Library
SurfaceByBoundary Object
Members 
Description
Represents an occurrence of a surface defined by input edges.
Object Model
SurfaceByBoundary ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionSuppressVariable ObjectApplication Object
Remarks
You can selectively specify that edges of the new surface be tangent to input edges.
See Also

SurfaceByBoundary Members