Solid Edge Part Type Library
GetFaultsOfBody Method
Returns number of primary faulty geometries.
Returns Array of faulty geometries.
Returns Number of secondary faulty geometries.
Returns Array of secondary faulty geometries.
Returns State of faulty geometries.
Returns Position of faulty geometries.
Description
Find faults in a body.
Syntax
Visual Basic
Public Sub GetFaultsOfBody( _
   ByRef NumPrimaryFaultGeometries As Long, _
   ByRef PrimaryFaultGeometries() As Object, _
   ByRef NumSecondaryFaultGeometries As Long, _
   ByRef SecondaryFaultGeometries() As Object, _
   ByRef FaultStates() As Long, _
   ByRef Positions() As Double _
) 
Parameters
NumPrimaryFaultGeometries
Returns number of primary faulty geometries.
PrimaryFaultGeometries
Returns Array of faulty geometries.
NumSecondaryFaultGeometries
Returns Number of secondary faulty geometries.
SecondaryFaultGeometries
Returns Array of secondary faulty geometries.
FaultStates
Returns State of faulty geometries.
Positions
Returns Position of faulty geometries.
Example
Imports System.Runtime.InteropServices
Public Class GetFaultsOfBody

    Private Sub Button1_Click(sender As Object, e As EventArgs) Handles Button1.Click
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDoc As SolidEdgePart.PartDocument = Nothing
        Dim objModels As SolidEdgePart.Models = Nothing
        Dim objModel As SolidEdgePart.Model = Nothing
        Dim objType As Type = Nothing

        Dim NumPrimaryFaultGeometries As Integer
        Dim PrimaryFaultGeometries(0 To 100) As Object
        Dim NumSecondaryFaultGeometries As Integer
        Dim SecondaryFaultGeometries(0 To 100) As Object
        Dim FaultStates(0 To 100) As Integer
        Dim Position(0 To 100) As Double
        NumPrimaryFaultGeometries = 0
        NumSecondaryFaultGeometries = 0

        Try
            ' Create/get the application with specific settings
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")

            If objApplication Is Nothing Then
                ' Get the type from the Solid Edge ProgID
                objType = Type.GetTypeFromProgID("SolidEdge.Application")
                ' Start Solid Edge
                objApplication = Activator.CreateInstance(objType)
                ' Make Solid Edge visible
                objApplication.Visible = True
            End If

            ' Get document
            objDoc = objApplication.ActiveDocument

            ' get the models collection
            objModels = objDoc.Models()
            objModel = objModels.Item(1)

            Call objModel.GetFaultsOfBody(NumPrimaryFaultGeometries,
                                     PrimaryFaultGeometries,
                                    NumSecondaryFaultGeometries,
                                    SecondaryFaultGeometries,
                                    FaultStates,
                                    Position)

        Catch ex As Exception
            MsgBox(ex.ToString)
        End Try
    End Sub
End Class
See Also

Model Object  | Model Members