Solid Edge Part Type Library
Model Object
Members 
Description
Represents a collection of features that define a single part.
Object Model
Model ObjectApplication ObjectSelectSet CollectionAddIns CollectionApplication ObjectApplicationEvents ObjectApplicationV8DocumentOpenEvent ObjectApplicationWindowEvents ObjectBeforeFileSaveAsEvents ObjectCommand ObjectCustomization ObjectDocuments CollectionEnvironments CollectionFeatureLibraryEvents ObjectFileUIEvents ObjectMatTable ObjectInsight ObjectNewFileUIEvents ObjectApplication ObjectSEECEvents ObjectSESPEvents ObjectShortcutMenuEvents ObjectSolidEdgeInsightXT ObjectSolidEdgeTCE ObjectWindows CollectionBeads CollectionBends CollectionBlankSurfaces CollectionBlends CollectionBooleanFeatures CollectionBoxFeatures CollectionBreakCorners CollectionChamfers CollectionChangeBendAngles CollectionCloseCorners CollectionContourFlanges CollectionConvertPartToSMCollection CollectionConvToSMs CollectionCopiedParts CollectionCrossBrakes CollectionCylinderFeatures CollectionDeleteBlends CollectionDeleteFaces CollectionDeleteHoles CollectionDeleteRegions CollectionDelSMFaces CollectionDimples CollectionDrafts CollectionDrawnCutouts CollectionEmbossFeatures CollectionEnclosures CollectionEtches CollectionExtrudedCutouts CollectionExtrudedProtrusions CollectionFaceMoves CollectionFaceOffsets CollectionFaceRotates CollectionFeatureGroups CollectionFeatures CollectionFlanges CollectionGussets CollectionHelixCutouts CollectionHelixProtrusions CollectionHems CollectionHoles CollectionIntersects CollectionJogs CollectionLips CollectionLiveSections CollectionLoftedCutouts CollectionLoftedFlanges CollectionLoftedProtrusions CollectionLouvers CollectionMatchFlangeFaces CollectionMirrorCopies CollectionMirrorParts CollectionModelRecomputeEvents ObjectMountingBossCollection CollectionNormalCutouts CollectionNormalToFaceCutouts CollectionNormalToFaceProtrusions CollectionOffsetEdges CollectionPartFilletWelds CollectionPartGrooveWelds CollectionPartingSplits CollectionPartLabelWelds CollectionPartStitchWelds CollectionPatternParts CollectionPatterns CollectionRebends CollectionRedefineFaces CollectionReplaceFaces CollectionResizeBends CollectionResizeHoles CollectionResizeRounds CollectionRevolvedCutouts CollectionRevolvedProtrusions CollectionRibs CollectionRipEdges CollectionRounds CollectionSlots CollectionSphereFeatures CollectionSplitFaces CollectionSplits CollectionSubtracts CollectionSweptCutouts CollectionSweptProtrusions CollectionTabs CollectionThickens CollectionThins CollectionThinwalls CollectionThreads CollectionTubeFeatures CollectionUnbends CollectionUnions CollectionUserDefinedPatterns CollectionVents CollectionWebNetworks CollectionWireFeatures Collection
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()

        Dim objApplication As SolidEdgeFramework.Application
        Dim objPartDocument As SolidEdgePart.PartDocument
        Dim objModels As SolidEdgePart.Models
        Dim objModel As SolidEdgePart.Model

        Try
            OleMessageFilter.Register()

            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objPartDocument = objApplication.ActiveDocument
            objModels = objPartDocument.Models
            objModel = objModels.Item(1)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

Model Members  | Solid Edge ST3 - What's New