Solid Edge Part Type Library > Models Collection : AddFiniteExtrudedProtrusion Method |
Visual Basic |
---|
Public Function AddFiniteExtrudedProtrusion( _ ByVal NumberOfProfiles As Long, _ ByRef ProfileArray() As Object, _ ByVal ProfilePlaneSide As FeaturePropertyConstants, _ ByVal ExtrusionDistance As Double, _ Optional ByVal KeyPointOrTangentFace As Variant, _ Optional ByVal KeyPointFlags As Variant, _ Optional ByVal FromSurfOrRefPlane As Variant, _ Optional ByVal ToSurfOrRefPlane As Variant _ ) As Model |
Value | Description |
---|---|
igAddRound | |
igAll | |
igAlongAnAxis | |
igAngularDummy | |
igAsConstruction | |
igBend | |
igBendAndFaceCornerRelief | |
igBendOnlyCornerRelief | |
igBoth | Feature Properties - Both |
igChainedCornerRelief | |
igChamfer2Setbacks | |
igChamfer45degSetback | |
igChamferAngleSetback | |
igCircular | |
igCloseCornerCircleCutout | |
igCloseCornerClosed | |
igCloseCornerNone | |
igCloseCornerOpen | |
igClosed | |
igCloseFaces | |
igConcave | |
igConstantRadiusArc | |
igConstRadiusRound | |
igContinuous | |
igConvex | |
igCopy | |
igCornerRound | |
igCounterboreHole | |
igCounterboreProfileIsAtBottom | |
igCounterboreProfileIsAtTop | |
igCounterdrillHole | |
igCountersinkHole | |
igCurvatureContinuous | |
igCurvatureContinuousInterior | |
igCurveSetSeperator | |
igDeleteFaceHeal | |
igDelSMFaceBoth | |
igDelSMFaceNone | |
igDelSystemRelief | |
igDelZeroBendRadius | |
igDevelopableSurface | |
igEdgeBasedCrossSection | |
igEdgesByLoop | |
igEdgesByVertex | |
igEnd | |
igEndCaps | |
igEqualOffset | |
igEquationType | |
igExtend | Feature Properties - Extend |
igExtendBendRelief | |
igFacesTouchingCurvesOnly | |
igFilletBendRelief | |
igFinite | |
igFlangeCenterOfEdge | |
igFlangeEndFromEndEdge | |
igFlangeEndOnEndEdge | |
igFlangeFromBothEndsOfEdge | |
igFlangeFromDefinedStartPoint | |
igFlangeFullEdge | |
igFlangeMatchFace | |
igFlangeOffset | |
igFlangeStartFromEndEdge | |
igFlangeStartOnEndEdge | |
igFlatten | |
igFormedEnd | |
igFromNonReferenceEnd | |
igFromReferenceEnd | |
igFromTo | |
igFull | |
igGroove | |
igHemTypeCenteredLoop | |
igHemTypeClosed | |
igHemTypeClosedLoop | |
igHemTypeCurl | |
igHemTypeOpen | |
igHemTypeOpenLoop | |
igHemTypeSFlange | |
igIgnoreBlends | |
igInside | Feature Properties - Remove/Add Material Inside |
igInsideDimension | |
igIntersect | |
igLancedEnd | |
igLeft | Feature Properties - Project to Left |
igLinear | |
igLinearCurvatureContinuousExtension | |
igLinearTangentExtension | |
igLip | |
igLouverFormedEndType | |
igLouverLancedEndType | |
igLouverRound | |
igLouverRoundNone | |
igMitreByAngle | |
igMitreByDist | |
igMitreManufacturingCut | |
igMitreNormalToThickness | |
igMitreParallelToThickness | |
igMitreRegularCut | |
igMove | |
igMultipleEdges | |
igNatural | |
igNeutralFactorFromExcel | |
igNFType | |
igNoCornerRound | |
igNoExtend | Feature Properties - Do Not Extend |
igNone | |
igNonSymmetric | |
igNormal | |
igNormalSideDummy | Feature Properties - Normal Side |
igNoRound | |
igNullConstant | |
igOffset | |
igOutside | Feature Properties - Remove/Add Material Outside |
igOutsideDimension | |
igOverlapFaces | |
igParallelDummy | |
igParallelToPlane | |
igPartingFromCurve | |
igPartingFromEdge | |
igPartingFromPlane | |
igPartingFromSurface | |
igPatternAlongCurve | |
igPatternByTable | |
igPatternCircular | |
igPatternFillRegion | |
igPatternMirror | |
igPatternMountingBoss | |
igPatternRectangular | |
igPatternUserDefined | |
igPeriodic | |
igProfileBasedCrossSection | |
igProjectOptionProject | |
igProjectOptionWrap | |
igPunchedEnd | |
igRadial | |
igRaisedCounterboreSlot | |
igRecessedCounterboreSlot | |
igRecreateBlends | |
igRectangularBendRelief | |
igReflective | |
igRegularHole | |
igRegularSlot | |
igRegularThread | |
igRemoveBoundaries | |
igRemoveExternalBoundaries | |
igRemoveInternalBoundaries | |
igReverseNormal | |
igReverseNormalSideDummy | Feature Properties - Reverse Normal Side |
igRight | Feature Properties - Project to Right |
igRipBendRelief | |
igRipCornerRelief | |
igRndCapAcrossSharpEdges | |
igRndMiterAtCorner | |
igRndPreserveTopologyOff | |
igRndPreserveTopologyOn | |
igRndRollAcrossSharpEdges | |
igRndRollAcrossTangentEdgesOff | |
igRndRollAcrossTangentEdgesOn | |
igRndRollAlongBlendEdgesOff | |
igRndRollAlongBlendEdgesOn | |
igRndRollAroundCorner | |
igRoundAllVertexSetback | |
igRoundEndVertexEdgeSetback | |
igRoundSetbackIsAbsolute | |
igRoundSetbackIsRelative | |
igRoundSingleVertexSetback | |
igRoundStartVertexEdgeSetback | |
igRoundVertexEdgeSetback | |
igShowBoundaries | |
igSideInfoSetSeperator | |
igSingleEdge | |
igSMClearanceCutout | |
igSMFaceCutout | |
igSMMidPlaneCutout | |
igSplit | |
igSplitAngle1Left | |
igSplitAngle1Right | |
igSplitDraft | |
igStart | |
igStepDraft | |
igStepDraftPerpendicular | |
igStraightPipeThread | |
igSubtract | |
igSweepAlignArcLength | |
igSweepAlignNormal | |
igSweepAlignParallel | |
igSweepAlignParametrically | |
igSweepC1Continuity | |
igSweepC2Continuity | |
igSweepMergeAll | |
igSweepMergeAlongPath | |
igSweepMergeNone | |
igSweepScaleNone | |
igSweepScaleStartAndEnd | |
igSweepTwistNone | |
igSweepTwistStartAndEnd | |
igSweepTwistTurns | |
igSweepTwistTurnsPerUnitLength | |
igSymmetric | Feature Properties - Symmetric Extent |
igTangent | |
igTangentInterior | |
igTaperByAngle | |
igTaperByRatio | |
igTaperByRLRatio | |
igTaperDimAtBottom | |
igTaperDimAtTop | |
igTaperedEnd | |
igTaperedHole | |
igTaperedPipeThread | |
igTaperedToPlane | |
igTappedHole | |
igThickness | |
igThkInProfilePlane | |
igThkNormalToProfilePlane | |
igThreeHundredAndSixty | |
igThroughAll | |
igThroughAxis | |
igToEndOfEdge | |
igToggleToConstruction | Toggle from Design to Construction |
igToggleToDesign | Toggle from Construction to Design |
igToKeyPoint | |
igToNext | |
igTreatmentCircleCutout | |
igTreatmentCrown | |
igTreatmentDraft | |
igTreatmentFormedFeatureDisplayAsCenterMark | |
igTreatmentFormedFeatureDisplayAsModeled | |
igTreatmentFormedFeatureDisplayAsSketch | |
igTreatmentFormedFeatureDisplayAsSketchAndCenterMark | |
igTreatmentIntersect | |
igTreatmentMiterRelief | |
igTreatmentOff | |
igTreatmentRectangularCutout | |
igTreatmentUCutout | |
igTreatmentVCutout | |
igUnequalOffset | |
igUnite | |
igUShaped | |
igVarRadiusRound | |
igVBottomDimToFlat | |
igVBottomDimToV | |
igVShaped | |
igWeldGrooveCapProject | |
igWeldGrooveCapSameAsTop | |
igWeldGrooveCapSurface |
Private Sub Form_Load() Dim objApp As SolidEdgeFramework.Application Dim objDoc As SolidEdgePart.PartDocument Dim objEPProfile As SolidEdgePart.Profile Dim objEPProfile01 As SolidEdgePart.Profile Dim objEPProfile02 As SolidEdgePart.Profile Dim objEPProfile03 As SolidEdgePart.Profile Dim objEPProfArray(1 To 3) As SolidEdgePart.Profile Dim objModel As SolidEdgePart.Model Dim objFromRP As SolidEdgePart.RefPlane Dim objToRP As SolidEdgePart.RefPlane Dim lngStatus As Long ' Report errors Const PI = 3.14159265358979 ' Create/get the application with specific settings On Error Resume Next Set objApp = GetObject(, "SolidEdge.Application") If Err Then Err.Clear Set objApp = CreateObject("SolidEdge.Application") Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument") objApp.Visible = True Else Set objDoc = objApp.ActiveDocument End If ' *** creating the base extruded protrusion feature symmetrically ' creating the profile and validating it Set objEPProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(1)) Call objEPProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.05) lngStatus = objEPProfile.End(ValidationCriteria:=igProfileClosed) If lngStatus <> 0 Then MsgBox "Profile for the base feature is not closed" End If ' creating the base extruded protrusion feature Set objEPProfArray(1) = objEPProfile Set objModel = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, _ ProfileArray:=objEPProfArray, ProfilePlaneSide:=igSymmetric, _ ExtrusionDistance:=0.1) 'Turn off the profile objEPProfile.Visible = False ' USER DISPLAY ' Release objects Set objApp = Nothing Set objDoc = Nothing Set objEPProfile = Nothing Set objEPProfArray(1) = Nothing Set objModel = Nothing Set objEPProfile01 = Nothing Set objEPProfile02 = Nothing Set objEPProfile03 = Nothing Set objFromRP = Nothing Set objToRP = Nothing End Sub