Solid Edge FrameworkSupport Type Library
WeldSymbolDataSet Object Members
Overview 
Public Properties
Public Property BottomNote1Sets and returns the Bottom Note 1 text for the referenced object.
Public Property BottomNote2Sets and returns the Bottom Note 2 text for the referenced object.
Public Property BottomNote3Sets and returns the Bottom Note 3 text for the referenced object.
Public Property BottomNoteZSets and returns the Bottom Note Z text for the referenced object.
Public Property BottomTreatmentTypeSets and returns the treatment display style to use for the bottom treatment portion of the referenced object.
Public Property BottomTypeSets and returns the bottom type for the referenced object.
Public Property BottomWeldModifierSets and returns the bottom weld modifier for the referenced object.
Public Property DashLineSets and returns the relative position of the dash lines for the referenced weld symbol object.
Public Property OffsetTopBottomSpecifies whether the top and bottom weld types are offset or aligned.
Public Property SymmetricalSpecifies whether or not the referenced object is symmetrical.
Public Property TailSpecifies whether the less than symbol appears at the end of the breaklline.
Public Property TailNoteSets and returns the tail note text.
Public Property TopNote1Sets and returns the Top Note 1 text.
Public Property TopNote2Sets and returns the Top Note 2 text.
Public Property TopNote3Sets and returns the Top Note 3 text.
Public Property TopNoteZSets and returns the Top Note Z text.
Public Property TopTreatmentTypeSets and returns the display style to use for the top treatment portion of the referenced object.
Public Property TopTypeSets and returns the top type for the referenced object.
Public Property TopWeldModifierSets and returns the top weld modifier for the referenced object.
Public Property WeldAllAroundSpecifies whether or not the 'weld all around' display style is included in the referenced object.
Public Property WeldInFieldSpecifies whether or not the 'weld in field' display style is included in the referenced object.
Public Property ZSymbolSpecifies whether or not the Z weld symbol modifier is included in the referenced object.
See Also

WeldSymbolDataSet Object