Solid Edge FrameworkSupport Type Library
WeldSymbolDataSet Object
Members 
Description
A collection of predefined Weld Symbol property settings.
Remarks
Each of these collection of settings is a data set. By adding a data set to the WeldSymbolDataSets collection object, those settings are available to the WeldSymbols collection object as a DataSet property selection. This property specifies the set of weld symbol characteristics on which to base a new WeldSymbol object.
See Also

WeldSymbolDataSet Members