Solid Edge FrameworkSupport Type Library
Smoothness Property
Collapse All
Expand All
Solid Edge FrameworkSupport Type Library
>
TextProfile Object
: Smoothness Property
Description
Returns the smoothness of the associated text. Range is [100,4500], where 100 is smoothest and 4500 is coarsest.
Property type
Read-only property
Syntax
Visual Basic
Public Property Smoothness As Integer
See Also
TextProfile Object
|
TextProfile Members