Solid Edge FrameworkSupport Type Library : TextProfile Object |
Copy | Places a copy of the referenced object on the clipboard. |
Cut | Moves the referenced object to the system clipboard. |
Delete | Deletes the referenced object. |
GetAlignment | Returns the justification (left, center, or right) of the line of text selected by the text line index. |
GetAnchorPoint | Returns the anchor point of the referenced TextProfile object. |
GetBoldState | Returns the bold state of the text character at the given index. |
GetCharCurveCount | Returns the number of curves in the character at the given index. |
GetCharStrokedCurveData | Returns stroked curve data of the curve at the given index of the character at the given index. |
GetItalicState | Returns the italic state of the text character at the given index. |
Move | Moves the referenced object. |
SetAnchorPoint | Sets the anchor point of the referenced TextProfile object. |
AnchorPointLocation | Returns the anchor point location of the referenced TextProfile object. |
Application | Returns the active application object. |
AttributeSets | Returns the AttributeSets collection object for the referenced object. |
FontName | Returns the name of the font. |
IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. |
LetterSpacing | Returns the spacing between letters for the associated text. |
LineSpacing | Returns the spacing between lines for the associated text. |
Margin | Returns the margin of the associated text. |
Parent | Returns the parent object for the referenced object. |
Smoothness | Returns the smoothness of the associated text. Range is [100,4500], where 100 is smoothest and 4500 is coarsest. |
Text | Returns the text of the referenced TextProfile object. |
TextSize | Returns the size of the associated text. |