Solid Edge FrameworkSupport Type Library
AddFeatureControlFrame Method
Description
Creates a FeatureControlFrame. For creating PMI FeatureControlFrame a plane must be set (XY plane is the default). The collection object from which it is derived (sheet/profile2d/PMI) dictate the creation of FeatureControlFrame.
Syntax
Visual Basic
Public Function AddFeatureControlFrame( _
   ByVal AnnotInitData As AnnotInitData _
) As FeatureControlFrame
Parameters
AnnotInitData
See Also

FeatureControlFrames Collection  | FeatureControlFrames Members  | Solid Edge ST5 - What's New