Public Methods
Add | Adds an occurrence of the referenced object. |
AddByTerminator | Creates a Leader or annotation object with a Leader. |
AddFeatureControlFrame | Creates a FeatureControlFrame. For creating PMI FeatureControlFrame a plane must be set (XY plane is the default). The collection object from which it is derived (sheet/profile2d/PMI) dictate the creation of FeatureControlFrame. |
ClearDataSet | Restores the property settings applied to existing annotation objects. |
ClearPlane | Clears any previously set plane object. |
ClearStyle | Clears any previously set style object. |
Item | The items in a collection. |
Public Properties
AnnotInitData | Initialization data object used for creating a new FeatureControlFrame using the AddFeatureControlFrame() API. |
Application | Returns the active application object. |
Count | Returns the number of objects in the referenced collection. |
DataSet | Sets and returns a previously saved set of property settings to apply to newly created annotation objects. |
Parent | Returns the parent object for the referenced object. |
Plane | For dimensions, returns the planar object used by the dimension to measure an object. For profiles, CopiedPart objects, and CopyConstruction objects, sets and returns the associated RefPlane object. |
Style | For collection objects, Body objects, RefPlane objects, Sketch objects, CoordinateSystem objects, CommandBarButton objects, SmartFrame2d objects, View objects, and TextCharStyle objects, Style is read-write. For all other objects, Style is read-only. |
See Also