Solid Edge Assembly Type Library
Color Property
Description
This read-write property sets or returns the color in which the active object is drawn. The color is stored as a long integer and is created with the RGB function (red, green, and blue color intensities) or as an integer between 0 and 16 that represents standard colors.
Property type
Read-write property
Syntax
Visual Basic
Public Property Color As Long
See Also

Wire Object  | Wire Members  | Solid Edge V18 - What's New