Solid Edge Assembly Type Library
Wire Object Members
Overview 
Public Methods
Public Method CreatePhysicalConductor
Public Method DeleteDeletes the referenced object.
Public Method DeletePhysicalConductor
Public Method Edit
Public Method GetAdders
Public Method GetAllPaths
Public Method GetEndPointsThis method returns the start and end points of the referenced object.
Public Method GetOuterConductors
Public Method GetPaths
Public Method GetTopMostConductors
Public Method Remove
Public Method SetAdders
Public Properties
Public Property ApplicationReturns the active application object.
Public Property AssemblyPropertyReturns the AssemblyProperty object used to store path attributes for the referenced object.
Public Property AttributeSetsReturns the AttributeSets collection object for the referenced object.
Public Property ColorThis read-write property sets or returns the color in which the active object is drawn. The color is stored as a long integer and is created with the RGB function (red, green, and blue color intensities) or as an integer between 0 and 16 that represents standard colors.
Public Property CutLength
Public Property Description
Public Property DiameterSets and returns the diameter of the referenced object.
Public Property FromComponentName
Public Property FromTerminalName
Public Property Gage
Public Property IsAttributeSetPresentReturns True if a specified Attribute Set exists on the referenced object.
Public Property LinearDensity
Public Property Mass
Public Property MaterialSets and returns the material.
Public Property MaterialType
Public Property MinimumBendRadius
Public Property NameReturns the name of the referenced object.
Public Property OuterDiameterSets and returns the outer diameter of the referenced object.
Public Property ParentReturns the parent object for the referenced object.
Public Property PartNumber
Public Property ToComponentName
Public Property ToTerminalName
Public Property TrueLength
Public Property TypeSpecifies the type of the object being referenced.
Public Property UseGlobalAdders
Public Property VisibleSpecifies whether or not the referenced object is displayed to the screen.
See Also

Wire Object  | Solid Edge V18 - What's New