Solid Edge Assembly Type Library
EndpointMagnitude Property
Description
Sets and returns the direction and degree of influence of the EndpointEdge on the curvature of the curve at the endpoint.
Property type
Read-only property
Syntax
Visual Basic
Public Property EndpointMagnitude As Double
Remarks
This value is meaningful only if the EndpointEndCondition is seKeypointEndConditionTangent.
See Also

Path Object  | Path Members  | Solid Edge V18 - What's New