Solid Edge Assembly Type Library : Path Object |
Delete | Deletes the referenced object. |
EditSpacePoint | |
GetAllPoints | |
GetEndPoints | This method returns the start and end points of the referenced object. |
GetFixedLength | Gives the fixed length of the path object. |
GetLength | |
InsertKeyPoint | Inserts a keypoint in the referenced curve before a specified point. |
InsertSpacePoint | |
InserttCylinderAxis | |
RemovePoint | Removes a keypoint from the curve for the referenced Path object. |
SetFixedLength | Sets fixed length of the path object. |
SplitPath | This method can split path of assembly path objects. |
Application | Returns the active application object. |
EndParentEdge | Sets and returns the Edge object from which the last keypoint in the curve was derived for the referenced Path object. |
EndpointEndCondition | Sets and returns the end condition of the last keypoint in the curve for the referenced Path object. |
EndpointMagnitude | Sets and returns the direction and degree of influence of the EndpointEdge on the curvature of the curve at the endpoint. |
Name | Returns the name of the referenced object. |
Parent | Returns the parent object for the referenced object. |
StartParentEdge | Sets and returns the Edge object from which the first keypoint in the curve was derived for the referenced Path object. |
StartpointEndCondition | Sets and returns the end condition of the first keypoint in the curve for the referenced Path object. |
StartpointMagnitude | Sets and returns the direction and degree of influence of the StartpointEdge on the curvature of the curve at the startpoint. |
Status | Returns the status of the specified object. |