Solid Edge Assembly Type Library
Add Method
Description
Adds an occurrence of the referenced object.
Syntax
Visual Basic
Public Function Add( _
   ByVal NumPoints As Long, _
   ByRef PointTypeConstants() As PointTypeConstants, _
   ByRef EdgeSet() As Object, _
   ByRef KeyPointTypeConstants() As KeyPointType, _
   ByRef Array() As Double, _
   ByVal StartpointEndType As KeypointEndConditionConstants, _
   Optional ByVal EndpointEndType As Variant _
) As Path
Parameters
NumPoints
PointTypeConstants
ValueDescription
igCylinderEndPoint
igCylinderStartPoint
igKeyPoint
igSpacePoint
EdgeSet
KeyPointTypeConstants
ValueDescription
igKeyPointCallbackKeypoint Type - Callback
igKeyPointCenterKeypoint Type - Center
igKeyPointEndKeypoint Type - End
igKeyPointHorizontalSilhouetteKeypoint Type - Horizontal Silhouette
igKeyPointInteriorNodeKeypoint Type - Interior Node
igKeyPointInteriorPoleKeypoint Type - Interior Pole
igKeyPointMajorAxisKeypoint Type - Major Axis
igKeyPointMiddleKeypoint Type - Middle
igKeyPointMinorAxisKeypoint Type - Minor Axis
igKeyPointNonDefiningKeypoint Type - Non-defining
igKeyPointPointOnlyKeypoint Type - Point Only
igKeyPointStartKeypoint Type - Start
igKeyPointVerticalSilhouetteKeypoint Type - Vertical Silhouette
Array
StartpointEndType
ValueDescription
seKeypointEndConditionCurvatureContinuousKeypoint End Condition - Curvature Continuous
seKeypointEndConditionNaturalKeypoint End Condition - Natural
seKeypointEndConditionNormalToFaceKeypoint End Condition - Normal To Face
seKeypointEndConditionPeriodicKeypoint End Condition - Periodic
seKeypointEndConditionTangentKeypoint End Condition - Tangent
EndpointEndType
See Also

Paths Collection  | Paths Members  | Solid Edge V18 - What's New