Solid Edge Assembly Type Library
Add Method
Description
Syntax
Visual Basic
Public Function Add( _
   ByVal NumberOfBaseFaces As Long, _
   ByRef BaseFaces() As Object, _
   ByVal NumberOfTargetFaces As Long, _
   ByRef TargetFaces() As Object, _
   ByVal pLabelWeldDataObject As Object, _
   ByVal eSetbackType As FilletWeldSetbackConstants, _
   ByVal dBaseThickness As Double, _
   ByVal dTargetThickness As Double _
) As AssemblyFilletWeld
Parameters
NumberOfBaseFaces
BaseFaces
NumberOfTargetFaces
TargetFaces
pLabelWeldDataObject
eSetbackType
ValueDescription
seFilletWeldEqualSetbackFilletBaseWidth is used for both base and target side fillet widths.
seFilletWeldThicknessFilletBaseWidth is used as the length of the perpendicular segment from the heel of the fillet to its opposite side.
seFilletWeldUnequalSetbackBase and target side fillet widths can be different.
dBaseThickness
dTargetThickness
See Also

AssemblyFilletWelds Collection  | AssemblyFilletWelds Members  | Solid Edge V18 - What's New