Solid Edge Part Type Library
FilletWeldSetbackConstants Enumeration
Description
Fillet Weld Setback Constants
Members
MemberValueDescription
seFilletWeldEqualSetback0FilletBaseWidth is used for both base and target side fillet widths.
seFilletWeldThickness2FilletBaseWidth is used as the length of the perpendicular segment from the heel of the fillet to its opposite side.
seFilletWeldUnequalSetback1Base and target side fillet widths can be different.