Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldFeatureSetType |
WeldFeatureSetType.ARC_SPOT
Arc Spot
|
static WeldFeatureSetType |
WeldFeatureSetType.BIW_DATUM_CUSTOMER1
Datum Customer1
|
static WeldFeatureSetType |
WeldFeatureSetType.BIW_DATUM_CUSTOMER2
Datum Customer2
|
static WeldFeatureSetType |
WeldFeatureSetType.BIW_DATUM_CUSTOMER3
Datum Customer3
|
static WeldFeatureSetType |
WeldFeatureSetType.BIW_DATUM_PIN
Datum Pin
|
static WeldFeatureSetType |
WeldFeatureSetType.BIW_DATUM_SURFACE
Datum Surface
|
static WeldFeatureSetType |
WeldFeatureSetType.BIW_MEASUREMENT_CUSTOMER1
Measurement Customer1
|
static WeldFeatureSetType |
WeldFeatureSetType.BIW_MEASUREMENT_CUSTOMER2
Measurement Customer2
|
static WeldFeatureSetType |
WeldFeatureSetType.BIW_MEASUREMENT_CUSTOMER3
Measurement Customer3
|
static WeldFeatureSetType |
WeldFeatureSetType.BIW_MEASUREMENT_HEM
Measurement Hem
|
static WeldFeatureSetType |
WeldFeatureSetType.BIW_MEASUREMENT_HOLE
Measurement Hole
|
static WeldFeatureSetType |
WeldFeatureSetType.BIW_MEASUREMENT_SLOT
Measurement Slot
|
static WeldFeatureSetType |
WeldFeatureSetType.BIW_MEASUREMENT_STUD
Measurement Stud
|
static WeldFeatureSetType |
WeldFeatureSetType.BIW_MEASUREMENT_SURFACE
Measurement Surface
|
static WeldFeatureSetType |
WeldFeatureSetType.BIW_MEASUREMENT_TRIM
Measurement Trim
|
static WeldFeatureSetType |
WeldFeatureSetType.CLINCH
Clinch
|
static WeldFeatureSetType |
WeldFeatureSetType.CUSTOM1POINT
Custom1 Point
|
static WeldFeatureSetType |
WeldFeatureSetType.CUSTOM2POINT
Custom2 Point
|
static WeldFeatureSetType |
WeldFeatureSetType.CUSTOM3POINT
Custom3 Point
|
static WeldFeatureSetType |
WeldFeatureSetType.CUSTOM4POINT
Custom4 Point
|
static WeldFeatureSetType |
WeldFeatureSetType.CUSTOM5POINT
Custom5 Point
|
static WeldFeatureSetType |
WeldFeatureSetType.DOLLOP
Dollop
|
static WeldFeatureSetType |
WeldFeatureSetType.FILLET_WELD
Fillet Weld
|
static WeldFeatureSetType |
WeldFeatureSetType.GROOVE_WELD
Groove Weld
|
static WeldFeatureSetType |
WeldFeatureSetType.RESISTANCE_SPOT
Resistance Spot
|
static WeldFeatureSetType |
WeldFeatureSetType.WELD_NUT
Weld Nut
|
static WeldFeatureSetType |
WeldFeatureSetType.WELD_STUD
Weld Stud
|
Modifier and Type | Method and Description |
---|---|
static WeldFeatureSetType |
WeldFeatureSetType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldFeatureSetType |
WeldFeatureSetType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldFeatureSetType[] |
WeldFeatureSetType.values()
Returns an array that contains the values for this enum.
|
WeldFeatureSetType |
WeldPointBuilder.weldType()
Returns the weld type.
|
WeldFeatureSetType |
AutoPointBuilder.weldType()
Deprecated.
Deprecated in NX10.0.0. Use overloaded function with PointMark enum instead.
|
Modifier and Type | Method and Description |
---|---|
void |
WeldPointBuilder.setWeldType(WeldFeatureSetType curWeldType)
Sets the weld type.
|
void |
AutoPointBuilder.setWeldType(WeldFeatureSetType weldPointType)
Deprecated.
Deprecated in NX10.0.0. Use overloaded function with PointMark enum instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.