Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Method and Description |
---|---|
WeldBeadSizeBuilder |
WeldBeadSizeBuilderList.findItem(int index)
Returns the object at the input index.
|
WeldBeadSizeBuilder[] |
WeldBeadSizeBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
WeldBeadSizeBuilder |
WeldBeadBuilder.newSize()
Creates a
WeldBeadSizeBuilder object. |
Modifier and Type | Method and Description |
---|---|
void |
WeldBeadSizeBuilderList.append(WeldBeadSizeBuilder object)
Appends an object to the list
License requirements: None. |
void |
WeldBeadSizeBuilderList.append(WeldBeadSizeBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
WeldBeadSizeBuilderList.erase(WeldBeadSizeBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
WeldBeadSizeBuilderList.erase(WeldBeadSizeBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
WeldBeadSizeBuilderList.findIndex(WeldBeadSizeBuilder obj)
Finds the index where the input object appears.
|
void |
WeldBeadSizeBuilderList.insert(int location,
WeldBeadSizeBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
WeldBeadSizeBuilderList.setContents(WeldBeadSizeBuilder[] objects)
Sets the contents of the entire list.
|
void |
WeldBeadSizeBuilderList.swap(WeldBeadSizeBuilder object1,
WeldBeadSizeBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.