Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldBeadSizeBuilder.TriangleTypes |
WeldBeadSizeBuilder.TriangleTypes.ONE_SIDED
Basically a right triangle
|
static WeldBeadSizeBuilder.TriangleTypes |
WeldBeadSizeBuilder.TriangleTypes.TWO_SIDED
Basically an isosceles triangle
|
Modifier and Type | Method and Description |
---|---|
WeldBeadSizeBuilder.TriangleTypes |
WeldBeadSizeBuilder.triangleType()
Returns the method used to indicate the type of triangle to create.
|
static WeldBeadSizeBuilder.TriangleTypes |
WeldBeadSizeBuilder.TriangleTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldBeadSizeBuilder.TriangleTypes |
WeldBeadSizeBuilder.TriangleTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldBeadSizeBuilder.TriangleTypes[] |
WeldBeadSizeBuilder.TriangleTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WeldBeadSizeBuilder.setTriangleType(WeldBeadSizeBuilder.TriangleTypes type)
License requirements: ugweld ("UG WELD") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.