Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Method and Description |
---|---|
WeldBeadPathBuilder |
WeldBeadPathBuilderList.findItem(int index)
Returns the object at the input index.
|
WeldBeadPathBuilder[] |
WeldBeadPathBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
WeldBeadPathBuilder |
WeldBeadBuilder.newPath()
Creates a
WeldBeadPathBuilder object. |
Modifier and Type | Method and Description |
---|---|
void |
WeldBeadPathBuilderList.append(WeldBeadPathBuilder object)
Appends an object to the list
License requirements: None. |
void |
WeldBeadPathBuilderList.append(WeldBeadPathBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
WeldBeadPathBuilderList.erase(WeldBeadPathBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
WeldBeadPathBuilderList.erase(WeldBeadPathBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
WeldBeadPathBuilderList.findIndex(WeldBeadPathBuilder obj)
Finds the index where the input object appears.
|
void |
WeldBeadPathBuilderList.insert(int location,
WeldBeadPathBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
WeldBeadPathBuilderList.setContents(WeldBeadPathBuilder[] objects)
Sets the contents of the entire list.
|
void |
WeldBeadPathBuilderList.swap(WeldBeadPathBuilder object1,
WeldBeadPathBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.