Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldArcMethod |
WeldArcMethod.CONTINUOUS
creates a single solid
|
static WeldArcMethod |
WeldArcMethod.SKIP
creates multiple solids
|
Modifier and Type | Method and Description |
---|---|
WeldArcMethod |
GrooveBuilder.method()
Deprecated.
Deprecated in NX9.0.0. Use
WeldGrooveBuilder.createSkipWelds() and WeldGrooveBuilder.setCreateSkipWelds(boolean) instead.
|
static WeldArcMethod |
WeldArcMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldArcMethod |
WeldArcMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldArcMethod[] |
WeldArcMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GrooveBuilder.setMethod(WeldArcMethod method)
Deprecated.
Deprecated in NX9.0.0. Use
WeldGrooveBuilder.createSkipWelds() and WeldGrooveBuilder.setCreateSkipWelds(boolean) instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.