Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Method and Description |
---|---|
JointmarkFaceSetsBuilder |
JointmarkFaceSetsBuilderList.findItem(int index)
Returns the object at the input index.
|
JointmarkFaceSetsBuilder[] |
JointmarkFaceSetsBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
JointmarkFaceSetsBuilder |
JointmarkBuilder.newFaceSets()
Creates a
JointmarkFaceSetsBuilder object. |
Modifier and Type | Method and Description |
---|---|
void |
JointmarkFaceSetsBuilderList.append(JointmarkFaceSetsBuilder object)
Appends an object to the list
License requirements: None. |
void |
JointmarkFaceSetsBuilderList.append(JointmarkFaceSetsBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
JointmarkFaceSetsBuilderList.erase(JointmarkFaceSetsBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
JointmarkFaceSetsBuilderList.erase(JointmarkFaceSetsBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
JointmarkFaceSetsBuilderList.findIndex(JointmarkFaceSetsBuilder obj)
Finds the index where the input object appears.
|
void |
JointmarkFaceSetsBuilderList.insert(int location,
JointmarkFaceSetsBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
JointmarkFaceSetsBuilderList.setContents(JointmarkFaceSetsBuilder[] objects)
Sets the contents of the entire list.
|
void |
JointmarkFaceSetsBuilderList.swap(JointmarkFaceSetsBuilder object1,
JointmarkFaceSetsBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.