Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static JointmarkBuilder.ReuseMethod |
JointmarkBuilder.ReuseMethod.ANY_CONNECTING_PARTS |
static JointmarkBuilder.ReuseMethod |
JointmarkBuilder.ReuseMethod.SAME_CONNECTING_PARTS |
Modifier and Type | Method and Description |
---|---|
JointmarkBuilder.ReuseMethod |
JointmarkBuilder.reuseFeaturesMethod()
Returns the method used to infer feature parameters if all connected parts are the same, or skip inferring due to connected parts being different.
|
static JointmarkBuilder.ReuseMethod |
JointmarkBuilder.ReuseMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static JointmarkBuilder.ReuseMethod |
JointmarkBuilder.ReuseMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static JointmarkBuilder.ReuseMethod[] |
JointmarkBuilder.ReuseMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
JointmarkBuilder.setReuseFeaturesMethod(JointmarkBuilder.ReuseMethod reuseMethod)
License requirements: ugweld ("UG WELD") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.