Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static JointmarkBuilder.ProjectionDirectionOptions |
JointmarkBuilder.ProjectionDirectionOptions.ALONG_FACE_NORMAL |
static JointmarkBuilder.ProjectionDirectionOptions |
JointmarkBuilder.ProjectionDirectionOptions.NONE |
static JointmarkBuilder.ProjectionDirectionOptions |
JointmarkBuilder.ProjectionDirectionOptions.PRICIPAL_AXIS |
static JointmarkBuilder.ProjectionDirectionOptions |
JointmarkBuilder.ProjectionDirectionOptions.X |
static JointmarkBuilder.ProjectionDirectionOptions |
JointmarkBuilder.ProjectionDirectionOptions.Y |
static JointmarkBuilder.ProjectionDirectionOptions |
JointmarkBuilder.ProjectionDirectionOptions.Z |
Modifier and Type | Method and Description |
---|---|
JointmarkBuilder.ProjectionDirectionOptions |
JointmarkBuilder.projectionDirectionOption()
Returns the projection direction option used to project
JointmarkBuilder.selectPointsObject() onto the JointmarkBuilder.getReferenceSheet() . |
static JointmarkBuilder.ProjectionDirectionOptions |
JointmarkBuilder.ProjectionDirectionOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static JointmarkBuilder.ProjectionDirectionOptions |
JointmarkBuilder.ProjectionDirectionOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static JointmarkBuilder.ProjectionDirectionOptions[] |
JointmarkBuilder.ProjectionDirectionOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
JointmarkBuilder.setProjectionDirectionOption(JointmarkBuilder.ProjectionDirectionOptions projectionOption)
License requirements: ugweld ("UG WELD") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.