Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static JointmarkBuilder.ConnectedPanelTypes |
JointmarkBuilder.ConnectedPanelTypes.FOUR |
static JointmarkBuilder.ConnectedPanelTypes |
JointmarkBuilder.ConnectedPanelTypes.THREE |
static JointmarkBuilder.ConnectedPanelTypes |
JointmarkBuilder.ConnectedPanelTypes.TWO |
Modifier and Type | Method and Description |
---|---|
JointmarkBuilder.ConnectedPanelTypes |
JointmarkBuilder.connectedPanelType()
Returns the number of connected panels at a point.
|
static JointmarkBuilder.ConnectedPanelTypes |
JointmarkBuilder.ConnectedPanelTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static JointmarkBuilder.ConnectedPanelTypes |
JointmarkBuilder.ConnectedPanelTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static JointmarkBuilder.ConnectedPanelTypes[] |
JointmarkBuilder.ConnectedPanelTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
JointmarkBuilder.setConnectedPanelType(JointmarkBuilder.ConnectedPanelTypes method)
License requirements: ugweld ("UG WELD") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.