Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static JointExitBuilder.Positions |
JointExitBuilder.Positions.LOWER
the lower position
|
static JointExitBuilder.Positions |
JointExitBuilder.Positions.LOWER_CHAMFER
the lower chamfer position
|
static JointExitBuilder.Positions |
JointExitBuilder.Positions.MIDDLE
the middle position
|
static JointExitBuilder.Positions |
JointExitBuilder.Positions.UPPER
the upper position
|
static JointExitBuilder.Positions |
JointExitBuilder.Positions.UPPER_CHAMFER
the upper chamfer position
|
Modifier and Type | Method and Description |
---|---|
static JointExitBuilder.Positions |
JointExitBuilder.Positions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static JointExitBuilder.Positions |
JointExitBuilder.Positions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static JointExitBuilder.Positions[] |
JointExitBuilder.Positions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
JointExitBuilder.EdgePrepValuesData |
JointExitBuilder.getEdgePrepValues(JointExitBuilder.Positions position)
Gets the thickness and angle combination to set for the desired weld position
License requirements: None. |
void |
JointExitBuilder.setEdgePrepValues(JointExitBuilder.Positions position,
double thickness,
double angle)
This method should be called multiple times.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.