Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static EdgePrepValuesBuilder.Option |
EdgePrepValuesBuilder.Option.COMPUTED
Use the computed values as edge prep values.
|
static EdgePrepValuesBuilder.Option |
EdgePrepValuesBuilder.Option.ENTERED
Use the values entered as edge prep values.
|
Modifier and Type | Method and Description |
---|---|
static EdgePrepValuesBuilder.Option |
EdgePrepValuesBuilder.Option.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EdgePrepValuesBuilder.Option |
EdgePrepValuesBuilder.Option.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EdgePrepValuesBuilder.Option[] |
EdgePrepValuesBuilder.Option.values()
Returns an array that contains the values for this enum.
|
EdgePrepValuesBuilder.Option |
EdgePrepValuesBuilder.valuesOption()
Returns the values option which indicates whether the entered or computed values should be used.
|
Modifier and Type | Method and Description |
---|---|
void |
EdgePrepValuesBuilder.setValuesOption(EdgePrepValuesBuilder.Option option)
License requirements: structure_weld ("STRUCTURE WELD") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.