Package | Description |
---|---|
nxopen.validate |
Provides classes and interfaces for Validation Utilities.
|
Modifier and Type | Field and Description |
---|---|
static RequirementBuilder.DefinitionMethodOptions |
RequirementBuilder.DefinitionMethodOptions.DOUBLE_SIDED_COMPARISON |
static RequirementBuilder.DefinitionMethodOptions |
RequirementBuilder.DefinitionMethodOptions.FORMULA |
static RequirementBuilder.DefinitionMethodOptions |
RequirementBuilder.DefinitionMethodOptions.SET_OF_VALUES |
static RequirementBuilder.DefinitionMethodOptions |
RequirementBuilder.DefinitionMethodOptions.SINGLE_SIDED_COMPARISON |
Modifier and Type | Method and Description |
---|---|
RequirementBuilder.DefinitionMethodOptions |
RequirementBuilder.definitionMethodOption()
Returns the definition method option
License requirements: None. |
static RequirementBuilder.DefinitionMethodOptions |
RequirementBuilder.DefinitionMethodOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RequirementBuilder.DefinitionMethodOptions |
RequirementBuilder.DefinitionMethodOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RequirementBuilder.DefinitionMethodOptions[] |
RequirementBuilder.DefinitionMethodOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RequirementBuilder.setDefinitionMethodOption(RequirementBuilder.DefinitionMethodOptions definitionMethodOption)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.