Package | Description |
---|---|
nxopen.userdefinedtemplate |
Provides classes and interfaces for User Defined Template.
|
Modifier and Type | Field and Description |
---|---|
static InstantiationBuilder.JaUserdefinedtemplateLayerOption |
InstantiationBuilder.JaUserdefinedtemplateLayerOption.ORIGINAL
Outputs will be in the same layer as in authoring part
|
static InstantiationBuilder.JaUserdefinedtemplateLayerOption |
InstantiationBuilder.JaUserdefinedtemplateLayerOption.SPECIFY
Outputs will be in user specified layer
|
static InstantiationBuilder.JaUserdefinedtemplateLayerOption |
InstantiationBuilder.JaUserdefinedtemplateLayerOption.WORK
Outputs will follow the work parts layer convention
|
Modifier and Type | Method and Description |
---|---|
InstantiationBuilder.JaUserdefinedtemplateLayerOption |
InstantiationBuilder.layerOption()
Returns the property of output layer option of User Defined Template instantiation
License requirements: None. |
static InstantiationBuilder.JaUserdefinedtemplateLayerOption |
InstantiationBuilder.JaUserdefinedtemplateLayerOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InstantiationBuilder.JaUserdefinedtemplateLayerOption |
InstantiationBuilder.JaUserdefinedtemplateLayerOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InstantiationBuilder.JaUserdefinedtemplateLayerOption[] |
InstantiationBuilder.JaUserdefinedtemplateLayerOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InstantiationBuilder.setLayerOption(InstantiationBuilder.JaUserdefinedtemplateLayerOption layerOption)
License requirements: usr_defined_features ("USER DEFINED FEATURES") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.