Package | Description |
---|---|
nxopen.sim |
Provides classes and interfaces for Machine Tool Builder and CAM-Simulation.
|
Modifier and Type | Method and Description |
---|---|
KinematicJunctionBuilder |
KinematicConfigurator.createJunctionBuilder(KinematicComponent parent,
KinematicJunction jct)
Creates a builder for a kinematic junction
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") OR nx_isv_mtb ("Machine Tool Builder") OR resource_manager_nx ("Teamcenter Resource Manager") . |
KinematicJunctionBuilder |
KinematicJunctionBuilderList.findItem(int index)
Returns the object at the input index.
|
KinematicJunctionBuilder[] |
KinematicJunctionBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
KinematicJunctionBuilderList.append(KinematicJunctionBuilder object)
Appends an object to the list
License requirements: None. |
void |
KinematicJunctionBuilderList.append(KinematicJunctionBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
KinematicJunctionBuilderList.erase(KinematicJunctionBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
KinematicJunctionBuilderList.erase(KinematicJunctionBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
KinematicJunctionBuilderList.findIndex(KinematicJunctionBuilder obj)
Finds the index where the input object appears.
|
void |
KinematicJunctionBuilderList.insert(int location,
KinematicJunctionBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
KinematicJunctionBuilderList.setContents(KinematicJunctionBuilder[] objects)
Sets the contents of the entire list.
|
void |
KinematicJunctionBuilderList.swap(KinematicJunctionBuilder object1,
KinematicJunctionBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.