Package | Description |
---|---|
nxopen.sim |
Provides classes and interfaces for Machine Tool Builder and CAM-Simulation.
|
Modifier and Type | Field and Description |
---|---|
static KinematicComponentBuilder.WorkPositionAngleTypes |
KinematicComponentBuilder.WorkPositionAngleTypes.NONE
no angle specified
|
static KinematicComponentBuilder.WorkPositionAngleTypes |
KinematicComponentBuilder.WorkPositionAngleTypes.SPECIFY_ANGLE
angle is specified
|
Modifier and Type | Method and Description |
---|---|
static KinematicComponentBuilder.WorkPositionAngleTypes |
KinematicComponentBuilder.WorkPositionAngleTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static KinematicComponentBuilder.WorkPositionAngleTypes |
KinematicComponentBuilder.WorkPositionAngleTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static KinematicComponentBuilder.WorkPositionAngleTypes[] |
KinematicComponentBuilder.WorkPositionAngleTypes.values()
Returns an array that contains the values for this enum.
|
KinematicComponentBuilder.WorkPositionAngleTypes |
KinematicComponentBuilder.workPositionAngleType()
Returns the working position angle type
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") OR nx_isv_mtb ("Machine Tool Builder") . |
Modifier and Type | Method and Description |
---|---|
void |
KinematicComponentBuilder.setWorkPositionAngleType(KinematicComponentBuilder.WorkPositionAngleTypes type)
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") OR nx_isv_mtb ("Machine Tool Builder") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.