Package | Description |
---|---|
nxopen.sim |
Provides classes and interfaces for Machine Tool Builder and CAM-Simulation.
|
Modifier and Type | Field and Description |
---|---|
static KinematicComponentBuilder.RegisterTypes |
KinematicComponentBuilder.RegisterTypes.SAME_AS_POCKET_ID
the pocket id defined the register
|
static KinematicComponentBuilder.RegisterTypes |
KinematicComponentBuilder.RegisterTypes.SPECIFY
the register is specified
|
Modifier and Type | Method and Description |
---|---|
KinematicComponentBuilder.RegisterTypes |
KinematicComponentBuilder.adjustRegisterType()
Returns the adjust register type
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") OR nx_isv_mtb ("Machine Tool Builder") . |
KinematicComponentBuilder.RegisterTypes |
KinematicComponentBuilder.cutcomRegisterType()
Returns the cutcom register type
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") OR nx_isv_mtb ("Machine Tool Builder") . |
static KinematicComponentBuilder.RegisterTypes |
KinematicComponentBuilder.RegisterTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static KinematicComponentBuilder.RegisterTypes |
KinematicComponentBuilder.RegisterTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static KinematicComponentBuilder.RegisterTypes[] |
KinematicComponentBuilder.RegisterTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
KinematicComponentBuilder.setAdjustRegisterType(KinematicComponentBuilder.RegisterTypes regType)
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") OR nx_isv_mtb ("Machine Tool Builder") . |
void |
KinematicComponentBuilder.setCutcomRegisterType(KinematicComponentBuilder.RegisterTypes regType)
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") OR nx_isv_mtb ("Machine Tool Builder") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.