Package | Description |
---|---|
nxopen.sim |
Provides classes and interfaces for Machine Tool Builder and CAM-Simulation.
|
Modifier and Type | Field and Description |
---|---|
static IsvControlPanelBuilder.DetailType |
IsvControlPanelBuilder.DetailType.COLLISION
Collision
|
static IsvControlPanelBuilder.DetailType |
IsvControlPanelBuilder.DetailType.GOUGE
Gouge
|
static IsvControlPanelBuilder.DetailType |
IsvControlPanelBuilder.DetailType.INFO
Info
|
static IsvControlPanelBuilder.DetailType |
IsvControlPanelBuilder.DetailType.LIMIT
Limit
|
static IsvControlPanelBuilder.DetailType |
IsvControlPanelBuilder.DetailType.SINGULARITY
Singularity
|
Modifier and Type | Method and Description |
---|---|
static IsvControlPanelBuilder.DetailType |
IsvControlPanelBuilder.DetailType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static IsvControlPanelBuilder.DetailType |
IsvControlPanelBuilder.DetailType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static IsvControlPanelBuilder.DetailType[] |
IsvControlPanelBuilder.DetailType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
IsvControlPanelBuilder.DetailData |
IsvControlPanelBuilder.getDetail(IsvControlPanelBuilder.DetailType type,
int position)
Return the Details Information to a specified type
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") . |
int |
IsvControlPanelBuilder.getDetailCount(IsvControlPanelBuilder.DetailType type)
Return the number of Details of the specified type
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.