public static class FlatPatternSettings.FlatPatternCalloutTypeDisplay extends Object implements Serializable
Modifier and Type | Field and Description |
---|---|
int |
isEnabled
Enabled status for the callout type.
|
String |
name
dialog name for the callout type.
|
String |
type
The name of the callout type.
|
Constructor and Description |
---|
FlatPatternCalloutTypeDisplay() |
FlatPatternCalloutTypeDisplay(String typeInitial,
int isEnabledInitial,
String nameInitial)
Constructor for the FlatPatternCalloutTypeDisplay object.
|
public String type
public int isEnabled
public String name
public FlatPatternCalloutTypeDisplay()
public FlatPatternCalloutTypeDisplay(String typeInitial, int isEnabledInitial, String nameInitial)
typeInitial
- The name of the callout type.
The string is one returned by the
get_callout_data method, or can
be hand-coded as the application name 'dot' the callout
name, like this:
"FlatPatternView.BendRadius". Neither name is
case sensitive and blanks are not significant. This type
of hand-coded callout type is usable as long as the
callout type name is unique within the application name.
Beware of changing the defaults and loading old parts.isEnabledInitial
- Enabled status for the callout type.nameInitial
- dialog name for the callout type.Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.