Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
nxopen.routing.electrical |
Provides classes and interfaces for Routing Electrical.
|
Modifier and Type | Method and Description |
---|---|
int |
CustomManager.AutoroutePlugin.autoroutePlugin(Connection[] connections)
This defines the prototype for the autoroute plugin.
|
Modifier and Type | Interface and Description |
---|---|
interface |
CableConnection
Connection used by a
CableDevice . |
interface |
JumperConnection
A jumper connection connects ports on the same connector.
|
interface |
NonPathConnection
Describes a connection that does not have a path
A pathless connection represents the abilitiy for objects to be connected even though there is not an explicit path between them. |
interface |
PathConnection
Describes a connection that has a path
From and To terminals are not coincident and need a path definition to be routable. |
Modifier and Type | Method and Description |
---|---|
Connection[] |
ConnectorDevice.findConnections()
Find connections.
|
Connection |
ElectricalStockDevice.findImplementedConnection()
Find the
Connection implemented by this device. |
Connection[] |
HarnessDefinition.getChildConnections()
Returns all of the Connection objects that are implemented by single devices
that are children of this harness
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") . |
Connection[] |
ConnectionCollection.getConnections()
Get Connections
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.