Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static SubdivideSegmentBuilder.Types |
SubdivideSegmentBuilder.Types.ARC_LENGTH_SEGMENTS
Arc Length Segments
|
static SubdivideSegmentBuilder.Types |
SubdivideSegmentBuilder.Types.AT_POINT
At Point
|
static SubdivideSegmentBuilder.Types |
SubdivideSegmentBuilder.Types.EQUAL_SEGMENTS
Equal Segments
|
Modifier and Type | Method and Description |
---|---|
SubdivideSegmentBuilder.Types |
SubdivideSegmentBuilder.type()
Returns the spacing method as
SubdivideSegmentBuilder.Types
License requirements: routing_base ("Routing Basic") Created in NX6.0.0 |
static SubdivideSegmentBuilder.Types |
SubdivideSegmentBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SubdivideSegmentBuilder.Types |
SubdivideSegmentBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SubdivideSegmentBuilder.Types[] |
SubdivideSegmentBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SubdivideSegmentBuilder.setType(SubdivideSegmentBuilder.Types type)
License requirements: routing_base ("Routing Basic") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.