Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Field and Description |
---|---|
static SplitDuctBuilder.FlowTypes |
SplitDuctBuilder.FlowTypes.ABSOLUTE_FLOW
Absolute flow
|
static SplitDuctBuilder.FlowTypes |
SplitDuctBuilder.FlowTypes.RELATIVE_FLOW
Relative flow
|
Modifier and Type | Method and Description |
---|---|
SplitDuctBuilder.FlowTypes |
SplitDuctBuilder.flowType()
Returns the type of flow to be displayed in the list flow column
License requirements: routing_hvac ("Routing HVAC") . |
static SplitDuctBuilder.FlowTypes |
SplitDuctBuilder.FlowTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SplitDuctBuilder.FlowTypes |
SplitDuctBuilder.FlowTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SplitDuctBuilder.FlowTypes[] |
SplitDuctBuilder.FlowTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SplitDuctBuilder.setFlowType(SplitDuctBuilder.FlowTypes flowType)
License requirements: routing_hvac ("Routing HVAC") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.