Package | Description |
---|---|
nxopen.routing |
Provides classes and interfaces for Routing.
|
nxopen.routing.electrical |
Provides classes and interfaces for Routing Electrical.
|
Modifier and Type | Interface and Description |
---|---|
interface |
StockDevice
The Routing StockDevice corresponds to a generic stock instance
of
SingleDevice . |
Modifier and Type | Method and Description |
---|---|
SingleDevice |
LogicalTerminal.getParentConnector()
The physical connector associated with the
Port . |
SingleDevice |
AssemblyDefinition.getReferencingDevice()
Gets the
SingleDevice object that has this AssemblyDefinition object as its definition. |
SingleDevice[] |
SingleDevice.getRelatedSingleDevices()
Assuming this single device to be the relating single device in a
DeviceRelationship , get associated related single devices. |
SingleDevice[] |
DeviceRelationship.getRelatedSingleDevices()
Returns the list of related
SingleDevice objects. |
SingleDevice |
SingleDevice.getRelatingSingleDevice()
Assuming this single device to be the related single device in a
DeviceRelationship , get associated relating single device. |
SingleDevice |
DeviceRelationship.getRelatingSingleDevice()
Returns the one
SingleDevice to which the other SingleDevice objects are related. |
SingleDevice[] |
AssemblyDefinition.getSingleDeviceChildren()
Gets the list of
SingleDevice objects contained in the assembly. |
Modifier and Type | Method and Description |
---|---|
void |
DeviceRelationship.addRelatedSingleDevice(SingleDevice relatedDevice)
Adds a
SingleDevice to the collection of related SingleDevice objects. |
void |
AssemblyDefinition.addSingleDeviceChild(SingleDevice device)
Adds a
SingleDevice object to the list of objects contained in the assembly. |
boolean |
AssemblyDefinition.isSingleDeviceChild(SingleDevice device)
Determines if a
SingleDevice object is contained in the assembly
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") Created in NX4.0.2 |
void |
DeviceRelationship.removeRelatedSingleDevice(SingleDevice relatedDevice)
Removes a
SingleDevice from the collection of related SingleDevice objects. |
void |
AssemblyDefinition.removeSingleDeviceChild(SingleDevice device)
Removes a
SingleDevice from the list of objects contained in the assembly. |
void |
DeviceRelationship.replaceRelatedSingleDevices(SingleDevice[] relatedDevices)
Replaces the collection of related
SingleDevice objects. |
void |
AssemblyDefinition.replaceSingleDeviceChildren(SingleDevice[] replacementChildren)
Replaces the list of
SingleDevice objects contained in the assembly. |
void |
DeviceRelationship.setRelatingSingleDevice(SingleDevice relatingDevice)
Sets the one Relating
SingleDevice . |
Modifier and Type | Interface and Description |
---|---|
interface |
CableDevice
Corresponds to a cable instance of an
ElectricalStockDevice . |
interface |
ConnectorDevice
The Electrical ConnectorDevice corresponds to a connector instance of
SingleDevice . |
interface |
ElectricalStockDevice
The Electrical Stock Device is a non instantiable superclass to classify
all electrical stock-based single devices.
|
interface |
HarnessDevice
The Electrical HarnessDevice corresponds to a harness instance of the
SingleDevice . |
interface |
ShieldDevice
The Electrical ShieldDevice corresponds to a shield instance of
ElectricalStockDevice . |
interface |
SystemDevice
The Electrical SystemDevice corresponds to a system instance of the
SingleDevice . |
interface |
WireDevice
The Electrical WireDevice corresponds to a wire instance of
ElectricalStockDevice . |
Modifier and Type | Method and Description |
---|---|
SingleDevice |
Connection.findNearestParentDevice()
Queries this connection for the nearest parent device.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.